SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
The sampling control and data capture is handled by the sample sequencers. All of the sequencers are identical in implementation except for the number of samples that can be captured and the depth of the FIFO. Table 10-1 shows the maximum number of samples that each sequencer can capture and its corresponding FIFO depth. Each sample that is captured is stored in the FIFO. In this implementation, each FIFO entry is a 32-bit word, with the lower 12 bits containing the conversion result.
| Sequencer | Number of Samples | Depth of FIFO |
|---|---|---|
| SS3 | 1 | 1 |
| SS2 | 4 | 4 |
| SS1 | 4 | 4 |
| SS0 | 8 | 8 |
For a given sample sequence, each sample is defined by bit fields in the ADC Sample Sequence Input Multiplexer Select (ADCSSMUXn), ADC Sample Sequence Extended Input Multiplexer Select (ADCSSEMUXn) and ADC Sample Sequence Control (ADCSSCTLn) registers, where "n" corresponds to the sequence number. The ADCSSMUXn and ADCSSEMUXn fields select the input pin, while the ADCSSCTLn fields contain the sample control bits corresponding to parameters such as temperature sensor selection, interrupt enable, end of sequence, and differential input mode. Sample sequencers are enabled by setting the respective ASENn bit in the ADC Active Sample Sequencer (ADCACTSS) register and should be configured before being enabled. Sampling is then initiated by setting the SSn bit in the ADC Processor Sample Sequence Initiate (ADCPSSI) register. In addition, sample sequences may be initiated on multiple ADC modules simultaneously using the GSYNC and SYNCWAIT bits in the ADCPSSI register during the configuration of each ADC module. For more information on using these bits, see Section 10.5.11.
When configuring a sample sequence, multiple uses of the same input pin within the same sequence are allowed. In the ADCSSCTLn register, the IEn bits can be set for any combination of samples, allowing interrupts to be generated after every sample in the sequence if necessary. Also, the END bit can be set at any point within a sample sequence. For example, if Sequencer 0 is used, the END bit can be set in the nibble associated with the fifth sample, allowing Sequencer 0 to complete execution of the sample sequence after the fifth sample.
After a sample sequence completes execution, the result data can be retrieved from the ADC Sample Sequence Result FIFO (ADCSSFIFOn) registers. The FIFOs are simple circular buffers that read a single address to pop result data. For software debug purposes, the positions of the FIFO head and tail pointers are visible in the ADC Sample Sequence FIFO Status (ADCSSFSTATn) registers along with FULL and EMPTY status flags. If a write is attempted when the FIFO is full, the write does not occur and an overflow condition is indicated. Overflow and underflow conditions are monitored using the ADCOSTAT and ADCUSTAT registers.