SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
Descriptions of exception handling use the following terms:
When the processor is executing an exception handler, an exception can preempt the exception handler if its priority is higher than the priority of the exception being handled. See Section 1.6.6 for more information about preemption by an interrupt. When one exception preempts another, the exceptions are called nested exceptions. See Section 1.6.7.1 for more information.
Return occurs when the exception handler is completed, and when there is no pending exception with sufficient priority to service and the completed exception handler was not handling a late-arriving exception. The processor pops the stack and restores the processor state to the state it had before the interrupt occurred. See Section 1.6.7.2 for more information.
This mechanism speeds up exception servicing. On completion of an exception handler, if a pending exception meets the requirements for exception entry, the stack pop is skipped and control transfers to the new exception handler.
This mechanism speeds up preemption. If a higher priority exception occurs during state saving for a previous exception, the processor switches to handle the higher-priority exception and initiates the vector fetch for that exception. State saving is not affected by late arrival because the saved state is the same for both exceptions. Therefore, the state saving continues uninterrupted. The processor can accept a late-arriving exception until the first instruction of the exception handler of the original exception enters the execute stage of the processor. When the late-arriving exception returns from the exception handler, the normal tail-chaining rules apply.