SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
The interrupt capabilities of each GPIO port are controlled by a set of seven registers. These registers are used to select the source of the interrupt, its polarity, and the edge properties. When one or more GPIO inputs cause an interrupt, a single interrupt output is sent to the interrupt controller for the entire GPIO port. For edge-triggered interrupts, software must clear the interrupt to enable any further interrupts. For a level-sensitive interrupt, the external source must hold the level constant for the interrupt to be recognized by the controller.
Three registers define the edge or sense that causes interrupts:
Interrupts are enabled/disabled via the GPIO Interrupt Mask (GPIOIM) register (see Section 17.5.6).
When an interrupt condition occurs, the state of the interrupt signal can be viewed in two locations: the GPIO Raw Interrupt Status (GPIORIS) and GPIO Masked Interrupt Status (GPIOMIS) registers (see Section 17.5.7 and Section 17.5.8). As the name implies, the GPIOMIS register only shows interrupt conditions that are allowed to be passed to the interrupt controller. The GPIORIS register indicates that a GPIO pin meets the conditions for an interrupt, but has not necessarily been sent to the interrupt controller.
For a GPIO level-detect interrupt, the interrupt signal generating the interrupt must be held until serviced. Once the input signal deasserts from the interrupt generating logical sense, the corresponding RIS bit in the GPIORIS register clears. For a GPIO edge-detect interrupt, the RIS bit in the GPIORIS register is cleared by writing a 1 to the corresponding bit in the GPIO Interrupt Clear (GPIOICR) register (seeSection 17.5.9). The corresponding GPIOMIS bit reflects the masked value of the RIS bit.
When programming the interrupt control registers (GPIOIS, GPIOIBE, or GPIOIEV), the interrupts should be masked (GPIOIM cleared). Writing any value to an interrupt control register can generate a spurious interrupt if the corresponding bits are enabled.