SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
If the CLKGATE bit in the EPIGPCFG register is clear, the EPI clock always toggles when General-purpose mode is enabled. If CLKGATE is set, the clock is output only when a transaction is occurring, otherwise the clock is held high. If the WR2CYC bit is clear, the EPI clock begins toggling 1 cycle before the WR strobe goes High. If the WR2CYC bit is set, the EPI clock begins toggling when the WR strobe goes High. The clock stops toggling after the first rising edge after the WR strobe is deasserted. The RD strobe operates in the same manner as the WR strobe when the WR2CYC bit is set. See Figure 16-28 and Figure 16-29.
Figure 16-28 EPI Clock Operation, CLKGATE = 1, WR2CYC = 0
Figure 16-29 EPI Clock Operation, CLKGATE = 1, WR2CYC = 1