SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
If several interrupts are pending, the CAN Interrupt (CANINT) register points to the pending interrupt with the highest priority, disregarding their chronological order. The status interrupt has the highest priority. Among the message interrupts, the message object's interrupt with the lowest message number has the highest priority. A message interrupt is cleared by clearing the message object's INTPND bit in the CANIFnMCTL register or by reading the CAN Status (CANSTS) register. The status Interrupt is cleared by reading the CANSTS register.
The interrupt identifier INTID in the CANINT register indicates the cause of the interrupt. When no interrupt is pending, the register reads as 0x0000. If the value of the INTID field is different from 0, then an interrupt is pending. If the IE bit is set in the CANCTL register, the interrupt line to the interrupt controller is active. The interrupt line remains active until the INTID field is 0, meaning that all interrupt sources have been cleared (the cause of the interrupt is reset), or until IE is cleared, which disables interrupts from the CAN controller.
The INTID field of the CANINT register points to the pending message interrupt with the highest interrupt priority. The SIE bit in the CANCTL register controls whether a change of the RXOK, TXOK, and LEC bits in the CANSTS register can cause an interrupt. The EIE bit in the CANCTL register controls whether a change of the BOFF and EWARN bits in the CANSTS register can cause an interrupt. The IE bit in the CANCTL register controls whether any interrupt from the CAN controller actually generates an interrupt to the interrupt controller. The CANINT register is updated even when the IE bit in the CANCTL register is clear, but the interrupt is not indicated to the CPU.
A value of 0x8000 (INTID = 0x8000, which means the interrupt identifier is a status interrupt) in the CANINT register indicates that an interrupt is pending because the CAN module has updated (but not necessarily changed) the CANSTS register, indicating that either an error or status interrupt has been generated. A write access to the CANSTS register can clear the RXOK, TXOK, and LEC bits in that same register; however, the only way to clear the source of a status interrupt is to read the CANSTS register.
The source of an interrupt can be determined in two ways during interrupt handling. The first is to read the INTID bit in the CANINT register to determine the highest priority interrupt that is pending, and the second is to read the CAN Message Interrupt Pending (CANMSGnINT) register to see all of the message objects that have pending interrupts.
An interrupt service routine reading the message that is the source of the interrupt may read the message and clear the INTPND bit of the message object at the same time by setting the CLRINTPND bit in the CANIFnCMSK register. Once the INTPND bit has been cleared, the CANINT register contains the message number for the next message object with a pending interrupt.