SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Figure 9-9 shows the CBC-MAC authentication mode of operation, where the input to the cryptographic core is XORed with the IV. The cryptographic core output is then fed back as IV for the next block. The last data input block is XORed with an additional input value stored in the temporary buffer; this can be any precalculated value and is dependent on the alignment of the last input block. The result is the cryptographic core output of the last encryption operation.
Figure 9-9 AES – CBC-MAC Authentication Mode