SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
When the CPU transfers the contents of a message object from a FIFO buffer by writing its number to the CANIFnCRQ register, the TXRQST and CLRINTPND bits in the CANIFnCMSK register should be set such that the NEWDAT and INTPEND bits in the CANIFnMCTL register are cleared after the read. The values of these bits in the CANIFnMCTL register always reflect the status of the message object before the bits are cleared. To assure the correct function of a FIFO buffer, the CPU should read out the message objects starting with the message object with the lowest message number. When reading from the FIFO buffer, the user should be aware that a new received message is placed in the message object with the lowest message number for which the NEWDAT bit of the CANIFnMCTL register is clear. As a result, the order of the received messages in the FIFO is not ensured.Figure 11-3 shows how a set of message objects which are concatenated to a FIFO Buffer can be handled by the CPU.
Figure 11-3 Message Objects in a FIFO Buffer