SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Flash DMA Starting Address (FLASHDMAST)
The starting address for the Flash region accessible by the µDMA is programmed in the FLASHDMAST register.
NOTE
The µDMA can access Flash in Run Mode only (not available in low power modes).
FLASHDMAST is shown in Figure 7-24 and described in Table 7-23.
Return to Summary Table.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | ADDR | ||||||||||||||
| R-0x0 | R/W-0x0 | ||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADDR | RESERVED | ||||||||||||||
| R/W-0x0 | R-0x0 | ||||||||||||||