SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
The common transmit FIFO is a 16-bit wide, 8-locations deep, first-in, first-out memory buffer. The CPU writes data to the FIFO by writing the SSI Data (SSIDR) register (see Section 23.5.3), and data is stored in the FIFO until it is read out by the transmission logic.
When configured as a master or a slave, parallel data is written into the transmit FIFO prior to a legacy SSI serial conversion and transmission to the attached slave or master, respectively, through the SSInDAT0/SSInTX pin.
In slave mode, the legacy SSI transmits data each time the master initiates a transaction. If the transmit FIFO is empty and the master initiates, the slave transmits the 8th most recent value in the transmit FIFO. If less than 8 values have been written to the transmit FIFO since the SSI module clock was enabled using the Rn bit in the RCGCSSI register or if the QSSI is reset using the SRSSI register, then 0 is transmitted. Care should be taken to ensure that valid data is in the FIFO as needed. The QSSI can be configured to generate an interrupt or a µDMA request when the FIFO is empty.
NOTE
When operating in Legacy Mode, the QuadSSI's SSInXDAT0 signal functions as SSInTX.