SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
The CPU may read a received message any time through the CAN interface registers, because the data consistency is ensured by the message handler state machine.
Typically, the CPU first writes 0x007F to the CANIFnCMSK register and then writes the number of the message object to the CANIFnCRQ register. That combination transfers the whole received message from the message RAM into the Message Buffer registers (CANIFnMSKn, CANIFnARBn, and CANIFnMCTL). Additionally, the NEWDAT and INTPND bits are cleared in the message RAM, acknowledging that the message has been read and clearing the pending interrupt generated by this message object.
If the message object uses masks for acceptance filtering, the CANIFnARBn registers show the full, unmasked ID for the received message.
The NEWDAT bit in the CANIFnMCTL register shows whether a new message has been received since the last time this message object was read. The MSGLST bit in the CANIFnMCTL register shows whether more than one message has been received since the last time this message object was read. MSGLST is not automatically cleared, and should be cleared by software after reading its status.
Using a remote frame, the CPU may request new data from another CAN node on the CAN bus. Setting the TXRQST bit of a receive object causes the transmission of a remote frame with the identifier of the receive object. This remote frame triggers the other CAN node to start the transmission of the matching data frame. If the matching data frame is received before the remote frame could be transmitted, the TXRQST bit is automatically reset. This prevents the possible loss of data when the other device on the CAN bus has already transmitted the data slightly earlier than expected.