SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Data transfers follow the format in Figure 19-4. After the START condition, a slave address is transmitted. This address is 7 bits long followed by an eighth bit, which is a data direction bit (R/S bit in the I2CMSA register). If the R/S bit is clear, it indicates a transmit operation (send), and if it is set, it indicates a request for data (receive). A data transfer is always terminated by a STOP condition generated by the master, however, a master can initiate communications with another device on the bus by generating a repeated START condition and addressing another slave without first generating a STOP condition. Various combinations of receive and transmit formats are then possible within a single transfer.
Figure 19-4 Complete Data Transfer With a 7-Bit Address The first seven bits of the first byte make up the slave address (see Figure 19-5). The eighth bit determines the direction of the message. A zero in the R/S position of the first byte means that the master transmits (sends) data to the selected slave, and a one in this position means that the master receives data from the slave.
Figure 19-5 R/S Bit in First Byte