SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
The two comparison values, COMP0 and COMP1, in the ADC Digital Comparator Range (ADCDCCMPn) register effectively break the conversion area into three distinct regions. These regions are referred to as the low-band (less than COMP0), mid-band (greater than COMP0 but less than or equal to COMP1), and high-band (greater than or equal to COMP1) regions. COMP0 and COMP1 may be programmed to the same value, effectively creating two regions, but COMP1 must always be greater than or equal to the value of COMP0. A COMP1 value that is less than COMP0 generates unpredictable results.