SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
NOTE
For rising-edge detection, the input signal must be high for at least two clock periods following the rising edge. Similarly, for falling-edge detection, the input signal must be low for at least two clock periods following the falling edge. Based on this criteria, the maximum input frequency for edge detection is 1/4 of the frequency.
In Edge-Count mode, the timer is configured as a 24-bit up- or down-counter including the optional prescaler with the upper count value stored in the GPTM Timer n Prescale (GPTMTnPR) register and the lower bits in the GPTMTnR register. In this mode, the timer is capable of capturing three types of events: rising edge, falling edge, or both. To place the timer in Edge-Count mode, the TnCMR bit of the GPTMTnMR register must be cleared. The type of edge that the timer counts is determined by the TnEVENT fields of the GPTMCTL register. During initialization in down-count mode, the GPTMTnMATCHR and GPTMTnPMR registers are configured so that the difference between the value in the GPTMTnILR and GPTMTnPR registers and the GPTMTnMATCHR and GPTMTnPMR registers equals the number of edge events that must be counted. In up-count mode, the timer counts from 0x0 to the value in the GPTMTnMATCHR and GPTMTnPMR registers. When executing an up count, that the value of GPTMTnPR and GPTMTnILR must be greater than the value of GPTMTnPMR and GPTMTnMATCHR. Table 18-6 lists the values that are loaded into the timer registers when the timer is enabled.
| Register | Count Down Mode | Count Up Mode |
|---|---|---|
| GPTMTnR | GPTMTnPR in combination with GPTMTnILR | 0x0 |
| GPTMTnV | GPTMTnPR in combination with GPTMTnILR | 0x0 |
When software writes the TnEN bit in the GPTM Control (GPTMCTL) register, the timer is enabled for event capture. Each input event on the CCP pin decrements or increments the counter by 1 until the event count matches GPTMTnMATCHR and GPTMTnPMR. When the counts match, the GPTM asserts the CnMRIS bit in the GPTM Raw Interrupt Status (GPTMRIS) register, and holds it until it is cleared by writing the GPTM Interrupt Clear (GPTMICR) register. If the capture mode match interrupt is enabled in the GPTM Interrupt Mask (GPTMIMR) register, the GPTM also sets the CnMMIS bit in the GPTM Masked Interrupt Status (GPTMMIS) register. In up-count mode, the current count of the input events is held in both the GPTMTnR and GPTMTnV registers. In down-count mode, the current count of the input events can be obtained by subtracting the GPTMTnR or GPTMTnV from the value made up of the GPTMTnPR and GPTMTnILR register combination.
In addition to generating interrupts, an ADC and/or a µDMA trigger can be generated. The ADC trigger is enabled by setting the TnOTE bit in GPTMCTL and the event that activates the ADC is configured in the GPTM ADC Event (GPTMADCEV) register. The µDMA trigger is enabled by configuring and enabling the appropriate µDMA channel as well as the type of trigger enable in the GPTM DMA Event (GPTMDMAEV) register (see Section 8.3.4).
After the match value is reached in down-count mode, the counter is then reloaded using the value in GPTMTnILR and GPTMTnPR registers, and stopped because the GPTM automatically clears the TnEN bit in the GPTMCTL register. Once the event count has been reached, all further events are ignored until TnEN is re-enabled by software. In up-count mode, the timer is reloaded with 0x0 and continues counting.
Figure 18-2 shows how Input Edge-Count mode works. In this case, the timer start value is set to GPTMTnILR = 0x000A and the match value is set to GPTMTnMATCHR = 0x0006 so that four edge events are counted. The counter is configured to detect both edges of the input signal.
The last two edges are not counted because the timer automatically clears the TnEN bit after the current count matches the value in the GPTMTnMATCHR register.
Figure 18-2 Input Edge-Count Mode Example, Counting Down