SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
To operate in the low-band region, the CIC field or the CTC field in the ADCDCCTLn register must be programmed to 0x0. This setting causes interrupts or triggers to be generated in the low-band region as defined by the programmed operational mode. An example of the state of the interrupt/trigger signal in the low-band region for each of the operational modes is shown in Figure 10-12. Note that a 0 in a column following the operational mode name (Always, Once, Hysteresis Always, and Hysteresis Once) indicates that the interrupt or trigger signal is deasserted and a 1 indicates that the signal is asserted.
Figure 10-12 Low-Band Operation (CIC = 0x0 or CTC = 0x0)