SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
A 32-word write buffer provides the capability to perform faster write accesses to the flash memory by programming two 32-bit words at a time, allowing 32 words to be programmed in the same time as 16 would take using the method described above. The data for the buffered write is written to the Flash Write Buffer (FWBn) registers.
The registers are 32-word aligned with flash memory, and therefore the register FWB0 corresponds with the address in FMA where bits [6:0] of FMA are all 0. FWB1 corresponds with the address in FMA + 0x4 and so on. Only the FWBn registers that have been updated since the previous buffered flash memory write operation are written. The Flash Write Buffer Valid (FWBVAL) register shows which registers have been written since the last buffered flash memory write operation. This register contains a bit for each of the 32 FWBn registers, where bit[n] of FWBVAL corresponds to FWBn. The FWBn register has been updated if the corresponding bit in the FWBVAL register is set.