SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
A BURST command is provided for the master module which allows a sequence of data transfers using the µDMA (or software, if desired) to handle the data in the FIFO. The BURST command is enabled by setting the BURST bit in the Master Control/Status (I2CMCS) register. The number of bytes transferred by a BURST request is programmed in the I2C Master Burst Length (I2CMBLEN) register and a copy of this value is automatically written to the I2C Master Burst Count (I2CMBCNT) register to be used as a down-counter during the BURST transfer. The bytes written to the I2C FIFO Data (I2CFIFODATA) register are transferred to the RX FIFO or TX FIFO depending on whether a transmit or receive is being executed. If data is NACKed during a BURST and the STOP bit is set in the I2CMCS register, the transfer terminates. If the STOP bit is not set, the software application must issue a repeated STOP or START when a NACK interrupt is asserted. In the case of a NACK, the I2CMBCNT register can be used to determine the amount of data that was transferred prior to the BURST termination. If the Address is NACKed during a transfer, then a STOP is issued.