SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Figure 9-10 shows one round of a GCM operation for encryption and decryption. A 32-bit counter is used as IV (as it is for CTR mode). The data is encrypted in the same way as in CTR mode, by XORing the cryptographic core output with the input. After the encryption or decryption, the ciphertext is XORed with the intermediate authentication result. The XORed result is used as input for the polynomial multiplication to create the next (intermediate) authentication result. For more information about the GCM protocol, see Section 9.2.3.2.1.
Figure 9-10 AES – GCM Operation