SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
When the USB OTG controller is ready to start a session, the SESSION bit must be set in the USBDEVCTL register. The USB OTG controller then enables ID pin sensing. The ID input is either taken Low if an A-type connection is detected or High if a B-type connection is detected. The DEV bit in the USBDEVCTL register is also set to indicate whether the USB OTG controller has adopted the role of the A device or the B device. As soon as the USB controller has detected that it is on the A side of the cable, it must enable VBUS power within 100ms or the USB controller reverts to device mode.
If the USB OTG controller is the A device, then the USB OTG controller enters host mode (the A device is always the default host), turns on VBUS, and waits for VBUS to go above the VBUS Valid threshold, as indicated by the VBUS bit in the USBDEVCTL register going to 0x3. The USB OTG controller then waits for a peripheral to be connected. When a peripheral is detected, a Connect interrupt is signaled and either the FSDEV or LSDEV bit in the USBDEVCTL register is set, depending whether a full-speed or a low-speed peripheral is detected. The USB controller then issues a RESET to the connected device. The SESSION bit in the USBDEVCTL register can be cleared to end a session. The USB OTG controller also automatically ends the session if babble is detected or if VBUS drops below session valid.
NOTE
The USB OTG controller may not remain in host mode when connected to high-current devices. Some devices draw enough current to momentarily drop VBUS below the VBUS-valid level causing the controller to drop out of host mode. The only way to get back into host mode is to allow VBUS to go below the Session End level. In this situation, the device is causing VBUS to drop repeatedly and pull VBUS back low the next time VBUS is enabled.
In addition, the USB OTG controller may not remain in host mode when a device is told that it can start using it's active configuration. At this point the device starts drawing more current and can also drop VBUS below VBUS valid.
If the USB OTG controller is the B device, then the USB OTG controller requests a session using the session request protocol defined in the USB On-The-Go supplement, that is, it first discharges VBUS. Then when VBUS has gone below the Session End threshold (VBUS bit in the USBDEVCTL register goes to 0x0) and the line state has been a single-ended zero for > 2 ms, the USB OTG controller pulses the data line, then pulses VBUS. At the end of the session, the SESSION bit is cleared either by the USB OTG controller or by the application software. The USB OTG controller then causes the PHY to switch out the pullup resistor on D+, signaling the A device to end the session.