| 31-16 |
RESERVED |
R |
0x0 |
|
| 15-14 |
ENUPD7 |
R/W |
0x0 |
MnPWM7 Enable Update Mode.
0x0 = ImmediateWrites to the PWM7EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM7EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM7EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 13-12 |
ENUPD6 |
R/W |
0x0 |
MnPWM6 Enable Update Mode.
0x0 = ImmediateWrites to the PWM6EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM6EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM6EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 11-10 |
ENUPD5 |
R/W |
0x0 |
MnPWM5 Enable Update Mode.
0x0 = ImmediateWrites to the PWM5EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM5EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM5EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 9-8 |
ENUPD4 |
R/W |
0x0 |
MnPWM4 Enable Update Mode.
0x0 = ImmediateWrites to the PWM4EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM4EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM4EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 7-6 |
ENUPD3 |
R/W |
0x0 |
MnPWM3 Enable Update Mode.
0x0 = ImmediateWrites to the PWM3EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM3EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM3EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 5-4 |
ENUPD2 |
R/W |
0x0 |
MnPWM2 Enable Update Mode.
0x0 = ImmediateWrites to the PWM2EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM2EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM2EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 3-2 |
ENUPD1 |
R/W |
0x0 |
MnPWM1 Enable Update Mode.
0x0 = ImmediateWrites to the PWM1EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM1EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM1EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|
| 1-0 |
ENUPD0 |
R/W |
0x0 |
MnPWM0 Enable Update Mode.
0x0 = ImmediateWrites to the PWM0EN bit in the PWMENABLE register are used by the PWM generator immediately.
0x1 = Reserved
0x2 = Locally SynchronizedWrites to the PWM0EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0.
0x3 = Globally SynchronizedWrites to the PWM0EN bit in the PWMENABLE register are used by the PWM generator the next time the counter is 0 after a synchronous update has been requested through the PWM Master Control (PWMCTL) register.
|