SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
Writing to a word in the alias region updates one bit in the bit-band region.
Bit 0 of the value written to a word in the alias region determines the value written to the targeted bit in the bit-band region. Writing a value with bit 0 set writes 1 to the bit-band bit, and writing a value with bit 0 clear writes 0 to the bit-band bit.
Bits 31:1 of the alias word have no effect on the bit-band bit. Writing 0x01 has the same effect as writing 0xFF. Writing 0x00 has the same effect as writing 0x0E.
When reading a word in the alias region, 0x0000.0000 indicates that the targeted bit in the bit-band region is clear and 0x0000.0001 indicates that the targeted bit in the bit-band region is set.