SLAU723A October 2017 ā October 2018 MSP432E401Y , MSP432E411Y
A fault condition is one in which the controller must be signaled to stop normal PWM function and then set the MnPWMn signals to a safe state. Two basic situations cause fault conditions:
The PWM generator can use the following inputs to generate a fault condition, including:
Fault conditions are calculated on a per-PWM generator basis. Each PWM generator configures the necessary conditions to indicate a fault condition exists. This method allows the development of applications with dependent and independent control.
Four fault input pins (MnFAULTn) are available. These inputs may be used with circuits that generate an active High or active Low signal to indicate an error condition. A MnFAULTn pins may be individually programmed for the appropriate logic sense using the PWMnFLTSEN register.
The PWM generator's mode control, including fault condition handling, is provided in the PWMnCTL register. This register determines whether the input or a combination of MnFAULTn input signals and/or digital comparator triggers (as configured by the PWMnFLTSRC0 and PWMnFLTSRC1 registers) is used to generate a fault condition. The PWMnCTL register also selects whether the fault condition is maintained as long as the external condition lasts or if it is latched until the fault condition until cleared by software. Finally, this register also enables a counter that may be used to extend the period of a fault condition for external events to assure that the duration is a minimum length. The minimum fault period count is specified in the PWMnMINFLTPER register.
NOTE
When using an ADC digital comparator as a fault source, the LATCH and MINFLTPER bits in the PWMnCTL register should be set to 1 to ensure trigger assertions are captured.
Status regarding the specific fault cause is provided in the PWMnFLTSTAT0 and PWMnFLTSTAT1 registers. Note that the fault status registers, PWMnFLTSTAT0 and PWMnFLTSTAT1, reflect the status of all fault sources, regardless of what fault sources are enabled for that particular generator.
PWM generator fault conditions may be promoted to a controller interrupt using the PWMINTEN register.