SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Power-Temp Brownout Control (PTBOCTL)
This register determines, based on an individual event level, the appropriate next level of action (for example, NONE, System Control Interrupt, NMI, or reset) when an event occurs.
Power-temperature event actions are directed to the core as a System Control Interrupt or NMI. When a reset occurs, its behavior is controlled by the Reset Behavior Control (RESBEHAVCTL) register. If one of the events configured in the PTBOCTL register causes a reset, it is registered as a BOR interrupt in the Reset Cause (RESC) register.
NOTE
VDDAis the supply voltage to the analog components of the device and VDD is the supply voltage to the digital components of the device.
PTBOCTL is shown in Figure 4-9 and described in Table 4-13.
Return to Summary Table.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0x0 | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0x0 | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | VDDA_UBOR | ||||||
| R-0x0 | R/W-0x0 | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VDD_UBOR | ||||||
| R-0x0 | R/W-0x3 | ||||||