All interrupts that are generated by the
WKUP_R5FSS are summarized in Module Integration, along with their mapping.
They can be divided into the following groups:
R5F CPU internal interrupts:
These are described in Arm Cortex-R5 Technical Reference Manual.
ECC аggregator interrupts: These
are described in the ECC Aggregator chapter.
RAT exception interrupt: This is
described in Section 7.2.2.6.