SPRUIV7C May 2022 – November 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
The ALE module allows Host Thread mapping based on any packet classification. That is the ALE can generate a thread ID used by the host based on ALE classifier matches.
When enabled the highest classifier match can map to a particular thread ID value.
The ALE also supports an optional default Thread ID value in the event that no classifier match.
Each Thread ID, including the default thread ID, has an enable functionality such that, if no classifier matches occur the default value is used, if the default is not enabled, the switch will use the {port,priority} value instead. If multiple classifier matches occur, the highest matching entry with a thread enable bit set will be used.
Three registers are used for ALE classification thread mapping configuration (CPSW3_CPSW_NU_ALE_THREADMAPDEF, CPSW3_CPSW_NU_ALE_THREADMAPCTL and CPSW3_CPSW_NU_ALE_THREADMAPVAL). The three thread mapping registers are used independently and are separate from the other ALE policing registers. The CPSW3_CPSW_NU_ALE_THREADMAPCTL register allows the CPSW3_CPSW_NU_ALE_THREADMAPVAL register contents to be written to the selected classifier. There is a CPSW3_CPSW_NU_ALE_THREADMAPDEF register that is used for all classifiers. The thread mapping registers can be written or changed at any time but any packets that are already processed will not have their thread altered.