SPRUIV7C May 2022 – November 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
Since AM62 is built on 36b physical address, there are memory regions beyond 4GB address, such as DDR data space and debug configuration space. This is not a problem for the ARM V8 core such as A53, since it supports up to 44b physical address. However, for the micro control processor such as M4F and R5, the processor only natively supports 32b physical address space. In order to allow those micro controllers accessing the full 36b physical address space, a region based remapping module is dedicated for each processor.