SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The RAT module performs a region based address translation. It translates a 32-bit input address into a 48-bit output address. Any input transaction that starts inside of a programmed region will have its address translated, if the region is enabled. Any disabled region is ignored from the translation lookup.
RAT has 16 regions, with each region having dedicated registers that define its attributes:
The input addresses are compared against all the enabled regions in parallel. The region size defines how many of the lowest address bits are included in the region space, starting from a 1B space to a 4GB space. Then the upper bits not part of the region are used for the lookup and comparison, matching those bits of the input addresses against the region base address. The region matches when it is enabled and the compare matches. The first region that matches has the output address set with the region translated base address upper bits. The lower bits that are part of the region size are copied from the input address to the output address. If there are no region matches then the input address is copied to the output address entirely.
RAT does not automatically correct transactions that cross region boundaries, that is, start inside of a region and end outside of it, or start outside of a region and end inside of it. If a boundary crossing transaction is detected, then RAT annuls the transaction as illegal, generates an interrupt and logs an error, as explained in Section 8.2.1.3, RAT Error Logging.
The region base address and translated base address must be aligned to the defined region size. For example, if the defined region size is 64KB, then the two addresses must be 64KB aligned. This is software responsibility as RAT does not perform such alignment check. Regions that are not aligned have unpredictable results.
Moreover, multiple region definitions must not overlap in their covered address space. RAT does not check for this, so it is software responsibility to take care of it. Overlapping regions may lead to unpredictable results.