SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
If the position counter is equal to QPOSMAX (in EQEP_QPOSMAX register), then the position counter is reset to 0 on the next EQEP clock for forward movement and position counter overflow flag is set. If the position counter is equal to 0, then the position counter is reset to QPOSMAX on the next QEP clock for reverse movement and position counter underflow flag is set. Figure 12-2314 shows the position counter reset operation in this mode.
First index marker is defined as the quadrature edge following the first index edge. The EQEP peripheral records the occurrence of the first index marker (EQEP_QEP_STS_CT[1] FIMF) and direction on the first index event marker (EQEP_QEP_STS_CT[6] FIDF); it also remembers the quadrature edge on the first index marker so that the same relative quadrature transition is used for the software index marker (EQEP_QDEC_QEP_CTL[21-20] IEL= 0b11).