SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Requests issued by the direct access controller, the indirect access controller or the STIG will be translated into a sequence of byte transfers to send downstream (before serialization to the FLASH device). These sequences depend on the requested transfer but an example of a typical 1-byte non sequential READ is shown below:
INSTRUCTION OPCODE -> ADDRESS -> Mode Byte -> Dummy Bytes -> 1 byte of don't care
For sequential accesses, an extra byte of data per read is pushed to the FLASH device on the back of the above sequence assuming it can be done so with no gap between each transferred byte.
When PHY mode is enabled and consequently no clock divider is configured, latency caused by multi domain synchronization may make an extra byte insufficient to avoid the transfer gap. To ensure the sequential access non-interrupted and keep the maximum performance of the controller, PHY Pipeline Mode is implemented. When enabled, number of don't care bytes is calculated based on the configuration.
The actual sequence sent to the FLASH device depends on the requested transfers, whether the transfer is non-sequential or sequential, whether the device has been configured in XIP mode and the state of the main Device Instruction Type programmable registers (OSPI_DEV_INSTR_RD_CONFIG_REG and OSPI_DEV_INSTR_WR_CONFIG_REG).
For writes, the write enable latch (or WEL) within the FLASH device itself must be high before a write sequence can be issued. The OSPI Flash Controller will automatically issue the write enable latch command before triggering a write command via the direct or indirect access controllers (DAC/INDAC) – that is the user does not need to perform this operation. For increasing flexibility and performance user can turn off this feature by setting the OSPI_DEV_INSTR_WR_CONFIG_REG[8] WEL_DIS_FLD bit. The opcode for WREN is typically 0x06 and is common between devices.
When write requests from the direct or indirect access controllers are no longer being received and all outstanding requests have been sent, the FLASH device will automatically start the page program write cycle. Any incoming request at this time will be held in wait states until the cycle has completed. The OSPI Flash Controller will automatically poll the FLASH device legacy SPI status register to identify when the write cycle has completed. This is achieved by sending the RDSR opcode to the FLASH device and waiting until the device itself has indicated the write cycle has completed (until the Write in Progress bit has cleared to zero and the write enable latch bit has also cleared to zero or device is ready bit has set to one). The WREN and the RDSR device instructions are the only ones that are sent by the controller under the hood. For any other specific instruction that the user determines should be sent to the device (for example if the device needs to be unprotected before a write command is issued), these should be handled separately by issuing FLASH commands via the STIG.
There is an option to trigger HOLD or RESET feature on I/Os of the Flash Device. The HOLD one is generally common across the devices and takes an alternative function of DQ3 pin (applicable when device operates neither in Quad SPI mode nor DDR). The transfer can be hold and then resumed by dedicated software trigger field (OSPI_CONFIG_REG[4] HOLD_PIN_FLD). The devices which have the HOLD feature on DQ3 usually need another dedicated pin for hardware reset and ones without HOLD feature usually have alternative reset on DQ3 what makes the additional reset pin being redundant. The controller supports both variants and reset selection register field (OSPI_CONFIG_REG[6] RESET_CFG_FLD) allows the user to configure which hardware reset solution is implemented in the device under usage.
After configuration is done, it is possible to trigger HOLD or RESET features using I/Os (OSPI_CONFIG_REG[4] HOLD_PIN_FLD or OSPI_CONFIG_REG[5] RESET_PIN_FLD bits). After HOLD activation the controller is introduced into waiting state and any other operations should not be requested before de-asserting of HOLD configuration bit. The HOLD feature is useful when any SPI transaction needs to be prolonged in order to adjust it into specific point in time. Note that any HOLD trigger issued during active SPI transaction may be synchronized into reference clock domain at the time the SPI transfer turns to be finished. In this case, there is nothing to hold so the low level SPI logic will not activate HOLD on DQ3. To check if HOLD request suspended the transfer OSPI_CONFIG_REG[31] IDLE_FLD bit can be polled for. If SPI is not in the IDLE state, the transfer was successfully suspended. It is important for the software to take care of resetting OSPI_CONFIG_REG[4] HOLD_PIN_FLD bit before newly triggered SPI transaction. In case HOLD request is set before the beginning of the transfer it will be HOLD right after it starts what may not always be a goal. The hardware RESET needs to be activated when CS is high (no valid transaction is present on SPI bus). It can be checked by polling of OSPI_CONFIG_REG[31]. If the controller is in the IDLE state and no other transfer requests are queued to perform, the hardware RESET can be triggered. The RESET feature is useful when any write, program or erase operation needs to be cancelled. No transfer request is permitted before driving the reset back to being inactive. Triggering HOLD or RESET on DQ3 at the time the device is configured to work in Quad SPI mode or DDR will overwrite transfer data on DQ3 with '0'. This behavior is considered as a software error so it is advisable for the system to make sure that the flash device was introduced to suitable SPI mode (that is by polling its configuration register) before triggering alternative DQ3 function. There are four independent reset outputs implemented to separate between multiple devices connected to the controller (up to 4 are supported). The decision which reset output is to be activated after triggering OSPI_CONFIG_REG[5] RESET_PIN_FLD bit is made based on OSPI_CONFIG_REG[9] PERIPH_SEL_DEC_FLD and OSPI_CONFIG_REG[13-10] PERIPH_CS_LINES_FLD bits. Reset output OSPI_ECC_VECTOR is to be directly driven into corresponding dedicated RESET pins of the devices with separated RESET pin and alternatively, Reset output OSPI_ECC_VECTOR is to be control OSPI_ECC_VECTOR of the DQ3 RESET devices enabling separating of DQ3 Controller Outputs on SoC integration level.
The controller supports all combinations of CPHA and CPOL for Serial Clock. It allows the controller to support any SPI target devices not limited to Flash Memories. Multiple-SPI flash devices use just a subset of these combinations depending on the Transfer Mode as defined in Table 12-3077.
| (SEL_CLK_POL_FLD, SEL_CLK_PHASE_FLD) | Edge Mode | Support |
| 0x00 (SPI MODE 0) | SDR | Yes |
| 0x01 (SPI MODE 1) | SDR | No |
| 0x10 (SPI MODE 2) | SDR | No |
| 0x11 (SPI MODE 3) | SDR | No |
| 0x00 (SPI MODE 0) | DDR | Yes |
| 0x01 (SPI MODE 1) | DDR | No |
| 0x10 (SPI MODE 2) | DDR | No |
| 0x11 (SPI MODE 3) | DDR | No |