SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
This PRU Event Interface directly feeds pulsed event information out of the PRU’s internal ALU. These events are exported out of the PRU_ICSSG and need to be connected to the system interrupt controller at the SoC level. The event interface can be used by the firmware to create software interrupts from the PRU to the Host processor.
Bit | Field | Description |
---|---|---|
31-6 | Reserved | |
5 | pru<n>_r31_vec_valid | Valid strobe for vector output |
4 | Reserved | |
3-0 | pru<n>_r31_vec[3:0] | Vector output |
Simultaneously writing a ‘1’ to pru<n>_r31_vec_valid (R31 bit 5) and a channel number from 0 to 15 to pru<n>_r31_vec[3:0] (R31 bits 3-0) creates a pulse on the output of the corresponding pr<k>_pru_mst_intr[x]_intr_req INTC system event. For example, writing ‘100000’ will generate a pulse on prk_pru_mst_intr[0]_intr_req, writing ‘100001’ will generate a pulse on prk_pru_mst_intr[1]_intr_req, and so on to where writing ‘101111’ will generate a pulse on prk_pru_mst_intr[15]_intr_req and writing ‘0xxxxx’ will not generate any system event pulses. The output values from both PRU cores in a subsystem are ORed together.
The output channels 0-15 are connected to the INTC system events 16-31, respectively. This allows the PRU to assert one of the system events 16-31 by writing to its own R31 register. The system event is used to either post a completion event to one of the host CPUs (Arm) or to signal the other PRU. The host to be signaled is determined by the system interrupt to interrupt channel mapping (programmable). The 16 events are named as prk_pru_mst_intr<15:0>_intr_req. See the PRU_ICSSG Interrupt Requests Mapping, in the section, PRU_ICSSG Local Interrupt Controller, for more details.