SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Data is automatically forwarded from the MII RX port to the MII TX port without manipulations, as shown in Figure 6-234. This configuration does not depend on the PRU core. However, it does support an option for PRU to snoop or monitor the received data through the RX L2, shown in Figure 6-235. The PRU does not access data and status bits through R31, and it does not modify and push data.
Figure 6-234 Auto-forward
Figure 6-235 Auto-forward with PRU Snoop