SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
At any time, if any interrupt is not to be propagated to the host, then that interrupt should be disabled. For disabling an interrupt whose interrupt number is N, write a 1h to the Nth bit in the interrupt enable clear registers (ICSS_INTC_ENABLE_CLR_REG0 to ICSS_INTC_ENABLE_CLR_REG4). Interrupt N can also be disabled by writing the value N in the interrupt enable clear index register (ICSS_INTC_ENABLE_CLR_INDEX_REG).