SPRUJ42E March 2022 – October 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
PRODUCTION DATA
Protocol Status Register. CAN protocol controller status, transmitter delay compensation value.
Return to Summary Table
| Instance Name | Physical Address |
|---|---|
| MCAN0 | 5260 8244h |
| MCAN1 | 5261 8244h |
| MCAN2 | 5262 8244h |
| MCAN3 | 5263 8244h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| NU27 | |||||||
| R | |||||||
| 0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| NU27 | TDCV | ||||||
| R | R | ||||||
| 0h | 0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| NU26 | PXE | RFDF | RBRS | RESI | DLEC | ||
| R | R | R | R | R | R | ||
| 0h | 0h | 0h | 0h | 0h | 7h | ||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| BO | EW | EP | ACT | LEC | |||
| R | R | R | R | R | |||
| 0h | 0h | 0h | 0h | 7h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:23 | NU27 | R | 0h | Reserved |
| 22:16 | TDCV | R | 0h | Transmitter Delay Compensation Value Position of the secondary sample point, defined by the sum of the measured delay from the MCAN TX to MCAN RX pins and the MCAN_TDCR[14-8] TDCO field. The SSP position is, in the data phase, the number of mtq between the start of the transmitted bit and the secondary sample point. Valid values are 0 to 127 mtq. |
| 15 | NU26 | R | 0h | Reserved |
| 14 | PXE | R | 0h | Protocol Exception Event 1'b0 = No protocol exception event occurred since last read access 1'b1 = Protocol exception event occurred |
| 13 | RFDF | R | 0h | Recieved a CAN FD Message This bit is set independent of acceptance filtering. 1'b0 = Since this bit was reset by the Host CPU, no CAN FD message has been received 1'b1 = Message in CAN FD format with FDF flag set has been received |
| 12 | RBRS | R | 0h | BRS flag of last recieved CAN FD Message This bit is set together with the MCAN_PSR[13] RFDF bit, independent of acceptance filtering. 1'b0 = Last received CAN FD message did not have its BRS flag set 1'b1 = Last received CAN FD message had its BRS flag set |
| 11 | RESI | R | 0h | ESI flag of last recieved CAN FD Message This bit is set together with the MCAN_PSR[13] RFDF bit, independent of acceptance filtering. 1'b0 = Last received CAN FD message did not have its ESI flag set 1'b1 = Last received CAN FD message had its ESI flag set |
| 10:8 | DLEC | R | 7h | Data Phase Last Error Code Type of last error that occurred in the data phase of a CAN FD format frame with its BRS flag set. Coding is the same as for the MCAN_PSR[2-0] LEC field. This field will be cleared to zero when a CAN FD format frame with its BRS flag set has been transferred (reception or transmission) without error. |
| 7 | BO | R | 0h | Bus_Off status 1'b0 = The MCAN module is not Bus_Off 1'b1 = The MCAN module is in Bus_Off state |
| 6 | EW | R | 0h | Warning Status 1'b0 = Both error counters are below the Error_Warning limit of 96 1'b1 = At least one of error counter has reached the Error_Warning limit of 96 |
| 5 | EP | R | 0h | Error Passive 1'b0 = The MCAN module is in the Error_Active state. It normally takes part in bus communication and sends an active error flag when an error has been detected 1'b1 = The MCAN module is in the Error_Passive state |
| 4:3 | ACT | R | 0h | Activity Monitors the module's CAN communication state. 2'b00 = Synchronizing - node is synchronizing on CAN communication 2'b01 = Idle - node is neither receiver nor transmitter 2'b10 = Receiver - node is operating as receiver 2'b11 = Transmitter - node is operating as transmitter Note: ACT is set to 0 by a Protocol Exception Event. |
| 2:0 | LEC | R | 7h | Last Error Code The MCAN_PSR[2-0] LEC field indicates the type of the last error to occur on the CAN bus. This field will be cleared to 0hwhen a message has been transferred (reception or transmission) without error. 3'b000 = No Error: No error occurred since the MCAN_PSR[2-0] LEC field has been reset by successful reception or transmission. 3'b001 = Stuff Error: More than 5 equal bits in a sequence have occurred in a part of a received message where this is not allowed. 3'b010 = Form Error: A fixed format part of a received frame has the wrong format. 3'b011 = AckError: The message transmitted by the MCAN module was not acknowledged by another node. 3'b100 = Bit1Error: During the transmission of a message (with the exception of the arbitration field), the device wanted to send a recessive level (bit of logical value '1'), but the monitored bus value was dominant. 3'b101 = Bit0Error: During the transmission of a message (or acknowledge bit, or active error flag, or overload flag), the device wanted to send a dominant level (data or identifier bit logical value 0), but the monitored bus value was recessive. During Bus_Off recovery this status is set each time a sequence of 11 recessive bits has been monitored. This enables the Host CPU to monitor the proceeding of the Bus_Off recovery sequence (indicating the bus is not stuck at dominant or continuously disturbed). 3'b110 = CRCError: The CRC check sum of a received message was incorrect. The CRC of an incom-ing message does not match with the CRC calculated from the received data. 3'b111 = NoChange: Any read access to the Protocol Status Register re-initializes the MCAN_PSR[2-0] LEC field to 3'b111. When the MCAN_PSR[2-0] LEC field shows the value 3'b111, no CAN bus event was detected since the last Host CPU read access to the Protocol Status Register. Note: When a frame in CAN FD format has reached the data phase with BRS flag set, the next CAN event (error or valid frame) will be shown in the MCAN_PSR[10-8] DLEC field instead of the MCAN_PSR[2-0] LEC field. An error in a fixed stuff bit of a CAN FD CRC sequence will be shown as a Form Error, not Stuff Error. |