SPRUJD4A December 2024 – November 2025 AM62D-Q1
In the xSPI boot mode, the ROM Code initializes the xSPI module and the image is read from the xSPI flash connected. If the image fails to be read correctly from offset 0x0 of the flash memory, the ROM will attempt to obtain the image at offset 0x400000. This is the only redundant image location supported by the ROM.