SPRUJD4A December 2024 – November 2025 AM62D-Q1
There are three GPIO modules in the device, which could generate almost 200 interrupts. Those GPIO interrupt outputs are routed to the GPIO interrupt router first before they are routed to the final interrupt destination. The GPIO interrupt router allows each output to select each GPIO interrupt independently.
The two GPIO modules in the Main domain use one GPIO interrupt router while the GPIO module in MCU domain has its own dedicated GPIO router. See Figure 10-7. See also Interrupts (Inputs) and Interrupts (Outputs).