SPRUJD4A December 2024 – November 2025 AM62D-Q1
The placement logic is a 2-stage queue which determines the order of commands that run in the DDR controller. The placement logic follows rules for determining placement of new commands into the queue, relative to the contents of the command queue at that time. Placement is determined by considering coherency, address collisions, source collisions, data collisions, user assigned priority, latency, age, and command type to offer low latency for critical controllers while optimizing bandwidth for all controllers. A second reordering stage allows ready-to-run commands to start even if the head-of-queue command is not yet ready to run. In addition, the queue can be disabled completely, resulting in an in-line queue that services requests in the order that they arrive.
The DDR controller also has a full look-ahead facility that reduces the effect of page misses by pre-conditioning rows for upcoming requests by using “spare” cycles in preceding transactions.