SPRUJD4A December 2024 – November 2025 AM62D-Q1
Any received packets with errors sent cut-thru from an Ethernet receive port to any Ethernet transmit port(s) will egress with at least one byte of the generated outgoing packet CRC inverted to indicate the error. This is due to the fact that cut-thru operations begin before the end of packet when the receive port determines that the packet had an error (long/code/align/CRC).
Any packet also sent cut-thru with the host included in the destination port mask will be dropped to the host (TXST_PKT_DROP) with the packet error indicated on TXST_PKT_ERR[3:0].
Any long/Jabber/Code/Align/CRC errored Ethernet received packet that is not actually sent cut-thru by the receive port will dropped unless CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_MAC_CONTROL_REG_k[22] RX_CEF_EN is set (which if set will cause the packet to be sent to the host port with the error indicated on TXST_PKT_ERR[3:0]. If a long/Jabber/Code/Align/CRC errored Ethernet received packet is sent cut-thru by the received port then a set CPSW3_CPSW_NU_CPSW_NU_ETH_MAC_i_PN_MAC_CONTROL_REG_k[22] RX_CEF_EN will not cause the errored packet to be sent to the host port since the packet has already been transferred to the destination ports.
The following cut-thru notes are valid: