SPRUJD4A December 2024 – November 2025 AM62D-Q1
There are separate TDM sequencers for the transmit section and the receive section. Each TDM sequencer keeps track of the slot count. In addition, the TDM sequencer checks the bits of the MCASP_RTDM/MCASP_XTDM register and determines if the MCASP should receive/transmit in that time slot.
There are two possibilities for a slot: The MCASP either performs Rx/Tx operations during the time slot (transmit/receive bit is active), or the MCASP skips Rx/Tx operations during the time slot (transmit/receive bit is inactive). In the latter case, no transfers between the XRBUF and XRSR registers in the serializer would occur during that time slot.
In addition, during time of inactive slots, the serializers programmed as transmitters place their data output pins - AXRn in a predetermined state - logic low, high, or high impedance (tri-stated) as programmed in each serializer control MCASP_SRCTLn[3-2] DISMOD register. Refer also to Section 12.1.1.4.9.2.1, TDM Time Slots Generation and Processing, for details on how DMA event or interrupt generations are handled during inactive time slots in TDM mode.
In case of a DIT-transmission (S/PDIF transfers): the time division multiplexing (TDM) sequencer is used to count the 384 subframes (slots) in the DIT block. If currently transmitting slot 1, slot 2 (next value of the TDM slot counter) should be used during the encode phase to select the appropriate C, V, and U bit, because the data encoded and written to a MCASP_XBUFn register during the current time slot (slot 1) is actually shifted out on the next time slot (n = 0 to 15).
The transmit TDM sequencer is controlled by the MCASP_XTDM register and reports the current transmit slot to the MCASP_XTDMSLOT[9-0] XSLOTCNT bit field.