SPRUJD4A December 2024 – November 2025 AM62D-Q1
The Host initiates a RX channel teardown by setting the tdown bit in the RT enable register for the target RX channel. The PDMA communicates the teardown state to the UDMA-P through the PSI-L data channel, to ensure that the teardown is not seen by the UDMA-P until all the previous PDMA data for the channel has been flushed.
The PDMA will not stop reading peripheral data until it reaches a FIFO boundary as configured through the 'X' and 'Y' parameters in the static TR. It will always attempt to complete the 'Y' count for the current event being processed. Upon reaching a stopping point, the PDMA will then clear the enable bit in the pairing register, however the teardown bit will remain set. No further packet processing will occur until the Host re-configures the channel. The teardown process will propagate to the UDMA-P and its final status can be checked there.