SPRUJF2A March 2026 – March 2026 AM13E23019
An ADC SOC event route is a fixed, point-to-point connection between a peripheral event publisher and the ADC peripheral, used to trigger start of conversions on the ADC module.
Standard Event Registers DMA_TRIGs
In the case of peripheral publishers that have the standard Event Management Registers, the route goes from the masked interrupt status (MIS) register to the ADC's start of conversion logic. When a conversion trigger is received by the ADC, the ADC acknowledges the request and the peripheral clears the request. The ADC also acknowledges the cleared request, after which a new request can be asserted by the peripheral.
IP-Specific Event Registers DMA_TRIGs
For publishing peripherals that implement a unique register set for managing ADC conversions, there is also unique logic used to configure each trigger condition. See the peripheral-specific section of this document for guidance on how to configure ADC trigger converions in this case.