SPRUJF2A March 2026 – March 2026
The receive interrupt flags for each peripheral specific UNICOMM instance are described below. These flags are raised when there is data present in the RX FIFO that is ready to be read by the CPU or DMA.
Below is the high-level sequence for receiving a fixed amount of data with interrupts.
Depending on the peripheral mode configured, additional steps before and/or after this sequence may be required to receive the data using the corresponding protocol. See the peripheral-specific UNICOMM chapters for more details about the software steps needed for each IP.