SPRUJF2A March 2026 – March 2026 AM13E23019
This feature allows sharing PGA_INM pin across three available PGA modules, which helps to save two pins for applications where multiple PGAs are required, but the PGA modules all can have a common negative sense point. To enable this feature, MMUXSEL and NMUXSEL must be set to 3 and 1, respectively. As you can see in Figure 17-12, PGA_NEG_SHARED is shared among three PGA modules internally so that the user can employ there PGA modules with only one inverting pin. In three-phase current measurement, three modules of PGA can be employed to monitor the shunt current by using only four pins. The schematic of three-phase current sensing is shown in Figure 17-13.