SPRUJF2A March 2026 – March 2026 AM13E23019
If a boot fails during execution of the boot configuration routine (BCR), SYSCTL asserts a BOOTRST to attempt another boot. A boot fail can be caused by the following:
Up to three attempts to successfully boot the device are made by hardware. If the first, second, or third boot attempt is successful, the application starts normally. If the third attempt fails, then the boot process fails, no further boot attempts are made, and the application software is not started.
The purpose of the additional boot attempts is to allow the device to boot correctly if a transient (temporary) error was the cause of the boot fail. If three boot attempts are not successful, a steady-state error condition is likely present and the application is not started to prevent unexpected operation.