SPRUJF2A March 2026 – March 2026 AM13E23019
The INTxCONT bits in the ADCINTSEL1N2 register configures how interrupts are handled when an ADCINTFLG has not yet been cleared from a prior interrupt. This mode is disabled by default and additional overlapping interrupts are not issued to the NVIC. By activating this mode, ADC interrupts always reach the NVIC. If interrupts occur while ADCINTFLG is set, the ADCINTOVF register remains set regardless of the configuration of the INTxCONT bits.