SPRUJF2A March 2026 – March 2026 AM13E23019
Table 21-35 lists the memory-mapped registers for the INPUT_FLAG_XBAR_REGS registers. All register offset addresses not listed in Table 21-35 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | XBARFLG1 | X-Bar Input Flag Register 1 | Go | |
| 4h | XBARFLG2 | X-Bar Input Flag Register 2 | Go | |
| 10h | XBARCLR1 | X-Bar Input Flag Clear Register 1 | Go | |
| 14h | XBARCLR2 | X-Bar Input Flag Clear Register 2 | Go |
Complex bit access types are encoded to fit into small table cells. Table 21-36 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W1C | W 1C | Write 1 to clear |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
XBARFLG1 is shown in Figure 21-25 and described in Table 21-37.
Return to the Summary Table.
X-Bar Input Flag Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| INPUTXBAR12 | INPUTXBAR11 | INPUTXBAR10 | INPUTXBAR9 | INPUTXBAR8 | INPUTXBAR7 | INPUTXBAR6 | INPUTXBAR5 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| INPUTXBAR4 | INPUTXBAR3 | INPUTXBAR2 | INPUTXBAR1 | ADC2EVT4 | ADC2EVT3 | ADC2EVT2 | ADC2EVT1 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| ADC1EVT4 | ADC1EVT3 | ADC1EVT2 | ADC1EVT1 | ADC0EVT4 | ADC0EVT3 | ADC0EVT2 | ADC0EVT1 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| CMPSS3_CTRIPL | CMPSS3_CTRIPH | CMPSS2_CTRIPL | CMPSS2_CTRIPH | CMPSS1_CTRIPL | CMPSS1_CTRIPH | CMPSS0_CTRIPL | CMPSS0_CTRIPH |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | INPUTXBAR12 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 30 | INPUTXBAR11 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 29 | INPUTXBAR10 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 28 | INPUTXBAR9 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 27 | INPUTXBAR8 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 26 | INPUTXBAR7 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 25 | INPUTXBAR6 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 24 | INPUTXBAR5 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 23 | INPUTXBAR4 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 22 | INPUTXBAR3 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 21 | INPUTXBAR2 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 20 | INPUTXBAR1 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 19 | ADC2EVT4 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 18 | ADC2EVT3 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 17 | ADC2EVT2 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 16 | ADC2EVT1 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 15 | ADC1EVT4 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 14 | ADC1EVT3 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 13 | ADC1EVT2 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 12 | ADC1EVT1 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 11 | ADC0EVT4 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 10 | ADC0EVT3 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 9 | ADC0EVT2 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 8 | ADC0EVT1 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 7 | CMPSS3_CTRIPL | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 6 | CMPSS3_CTRIPH | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 5 | CMPSS2_CTRIPL | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 4 | CMPSS2_CTRIPH | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 3 | CMPSS1_CTRIPL | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 2 | CMPSS1_CTRIPH | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 1 | CMPSS0_CTRIPL | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 0 | CMPSS0_CTRIPH | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
XBARFLG2 is shown in Figure 21-26 and described in Table 21-38.
Return to the Summary Table.
X-Bar Input Flag Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | EQEP2_STROBE_SYNCOUT | EQEP2_INDEX_SYNCOUT | EQEP1_STROBE_SYNCOUT | EQEP1_INDEX_SYNCOUT | EQEP0_STROBE_SYNCOUT | ||
| R-0-0h | R-0h | R-0h | R-0h | R-0h | R-0h | ||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| EQEP0_INDEX_SYNCOUT | EQEP2_ERR | EQEP1_ERR | EQEP0_ERR | MCAN0_FEVT2 | MCAN0_FEVT1 | MCAN0_FEVT0 | EXTSYNCOUT |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADCSOCB | ADCSOCA | ECAP1_OUT | ECAP0_OUT | INPUTXBAR16 | INPUTXBAR15 | INPUTXBAR14 | INPUTXBAR13 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-21 | RESERVED | R-0 | 0h | Reserved |
| 20 | EQEP2_STROBE_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 19 | EQEP2_INDEX_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 18 | EQEP1_STROBE_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 17 | EQEP1_INDEX_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 16 | EQEP0_STROBE_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 15 | EQEP0_INDEX_SYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 14 | EQEP2_ERR | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 13 | EQEP1_ERR | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 12 | EQEP0_ERR | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 11 | MCAN0_FEVT2 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 10 | MCAN0_FEVT1 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 9 | MCAN0_FEVT0 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 8 | EXTSYNCOUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 7 | ADCSOCB | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 6 | ADCSOCA | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 5 | ECAP1_OUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 4 | ECAP0_OUT | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 3 | INPUTXBAR16 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 2 | INPUTXBAR15 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 1 | INPUTXBAR14 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
| 0 | INPUTXBAR13 | R | 0h | This register is used to Flag the inputs of the X-Bars to provide software knowledge of the input sources which got triggered. 1: Corresponding Input was triggered 0: Corresponding Input was not triggered Note: [1] setting of this bit has priority over clear by software Reset type: CPU1.SYSRSn |
XBARCLR1 is shown in Figure 21-27 and described in Table 21-39.
Return to the Summary Table.
X-Bar Input Flag Clear Register 1
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| INPUTXBAR12 | INPUTXBAR11 | INPUTXBAR10 | INPUTXBAR9 | INPUTXBAR8 | INPUTXBAR7 | INPUTXBAR6 | INPUTXBAR5 |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| INPUTXBAR4 | INPUTXBAR3 | INPUTXBAR2 | INPUTXBAR1 | ADC2EVT4 | ADC2EVT3 | ADC2EVT2 | ADC2EVT1 |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| ADC1EVT4 | ADC1EVT3 | ADC1EVT2 | ADC1EVT1 | ADC0EVT4 | ADC0EVT3 | ADC0EVT2 | ADC0EVT1 |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| CMPSS3_CTRIPL | CMPSS3_CTRIPH | CMPSS2_CTRIPL | CMPSS2_CTRIPH | CMPSS1_CTRIPL | CMPSS1_CTRIPH | CMPSS0_CTRIPL | CMPSS0_CTRIPH |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | INPUTXBAR12 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 30 | INPUTXBAR11 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 29 | INPUTXBAR10 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 28 | INPUTXBAR9 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 27 | INPUTXBAR8 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 26 | INPUTXBAR7 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 25 | INPUTXBAR6 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 24 | INPUTXBAR5 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 23 | INPUTXBAR4 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 22 | INPUTXBAR3 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 21 | INPUTXBAR2 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 20 | INPUTXBAR1 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 19 | ADC2EVT4 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 18 | ADC2EVT3 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 17 | ADC2EVT2 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 16 | ADC2EVT1 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 15 | ADC1EVT4 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 14 | ADC1EVT3 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 13 | ADC1EVT2 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 12 | ADC1EVT1 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 11 | ADC0EVT4 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 10 | ADC0EVT3 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 9 | ADC0EVT2 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 8 | ADC0EVT1 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 7 | CMPSS3_CTRIPL | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 6 | CMPSS3_CTRIPH | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 5 | CMPSS2_CTRIPL | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 4 | CMPSS2_CTRIPH | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 3 | CMPSS1_CTRIPL | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 2 | CMPSS1_CTRIPH | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 1 | CMPSS0_CTRIPL | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 0 | CMPSS0_CTRIPH | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG1 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
XBARCLR2 is shown in Figure 21-28 and described in Table 21-40.
Return to the Summary Table.
X-Bar Input Flag Clear Register 2
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | EQEP2_STROBE_SYNCOUT | EQEP2_INDEX_SYNCOUT | EQEP1_STROBE_SYNCOUT | EQEP1_INDEX_SYNCOUT | EQEP0_STROBE_SYNCOUT | ||
| R-0-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | ||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| EQEP0_INDEX_SYNCOUT | EQEP2_ERR | EQEP1_ERR | EQEP0_ERR | MCAN0_FEVT2 | MCAN0_FEVT1 | MCAN0_FEVT0 | EXTSYNCOUT |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADCSOCB | ADCSOCA | ECAP1_OUT | ECAP0_OUT | INPUTXBAR16 | INPUTXBAR15 | INPUTXBAR14 | INPUTXBAR13 |
| R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h | R-0/W1C-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-21 | RESERVED | R-0 | 0h | Reserved |
| 20 | EQEP2_STROBE_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 19 | EQEP2_INDEX_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 18 | EQEP1_STROBE_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 17 | EQEP1_INDEX_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 16 | EQEP0_STROBE_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 15 | EQEP0_INDEX_SYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 14 | EQEP2_ERR | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 13 | EQEP1_ERR | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 12 | EQEP0_ERR | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 11 | MCAN0_FEVT2 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 10 | MCAN0_FEVT1 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 9 | MCAN0_FEVT0 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 8 | EXTSYNCOUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 7 | ADCSOCB | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 6 | ADCSOCA | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 5 | ECAP1_OUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 4 | ECAP0_OUT | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 3 | INPUTXBAR16 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 2 | INPUTXBAR15 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 1 | INPUTXBAR14 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |
| 0 | INPUTXBAR13 | R-0/W1C | 0h | Writing 1 to a bit in this register clears the corresponding bit in the XBARFLG2 register. Writing 0 has no effect Reset type: CPU1.SYSRSn |