SPRUJF2A March 2026 – March 2026 AM13E23019
The following example configures two SOCs each on ADCA and with identical trigger select and ACQPS values. This results in synchronous operation between ADCA and . For devices with more than two ADCs, the same principles can be used to synchronize all the ADCs.
Several things can be noted from Figure 15-14. First, while the ACQPS values must be the same for SOCs with the same number, different ACQPS values can be used for SOCs with different numbers. Because of this, synchronous operation does not require one global S+H time, but instead only channels sampled simultaneously require identical S+H durations. Another important point from this example is that any channel select value can be used for any SOC. If high-priority SOCs are to be used, the priority must be configured the same on all ADCs.