The GPIO module evaluates the state of input pins at the ULPCLK (PD0 bus clock) rate, synchronizing the pin state to ULPCLK through a 2-stage synchronizer before passing the GPIO state to the input glitch filter.
A programmable input glitch filter is provided for suppressing noise on digital input pins. The glitch filter runs at ULPCLK rate. Four levels of user-specified input filtering are possible:
- Sampled input without filtering (the minimum reliably detected pulse width is one ULPCLK cycle due to synchronization)
- Synchronized inputs which are not greater than 1 ULPCLK periods are filtered out (glitch filter value of >1)
- Synchronized inputs which are not greater than 3 ULPCLK periods are filtered out (glitch filter value of >3)
- Synchronized inputs which are not greater than 8 ULPCLK periods are filtered out (glitch filter value of >8)
Note: Inputs are synchronized to ULPCLK, causing up to one ULPCLK cycle of uncertainty in the synchronization. Input signals that are shorter than one ULPCLK cycle can be missed.
Note: For pins with fast wake enable, there is an input delay time equal to the time between the edge of the un-synchronized input edge to the first MCLK edge in STANDBY0/1, STOP1/2 and SLEEP2 modes.
This feature allows users to easily implement input filtering in hardware for cases where fast switching on the input pin is needed to be filtered out. The bit fields in the FILTEREN31_16 and FILTEREN15_0 registers allow users to configure the level of filtering needed for the corresponding GPIO bit.
Input pulses of the same pulse length can be passed in some cases while being filtered in other cases due to the uncertainty in synchronization. GPIO Input Synchronizer and Glitch Filtering Scenarios demonstrates different scenarios and how synchronization affects input detection.
- In Scenario A, the input pulse is less than one ULPCLK cycle. Pulses less than one ULPCLK cycle may not be captured. To ensure that GPIO inputs are always captured, the GPIO input pulse width must be greater than the ULPCLK period.
- In Scenario B, the input pulse is nearly two ULPCLK cycles in length, but because the rising edge occurs just after the ULPCLK edge, the GPIO synchronizer only views the input pin as having been high for 1 ULPCLK period. This scenario would not be filtered out by the glitch filter when the glitch filter is disabled, but a glitch filter value of >1 would result in this pulse being filtered. Conversely, the same input pulse width in Scenario C results in the input pin being considered high for two ULPCLK periods, as the rising edge occurred just before the ULPCLK edge. In this case, this scenario would not be filtered out when a glitch filter value of >1 is specified.
- In Scenario D, three ULPCLK cycles are passed to the glitch filter. In this case, the scenario would not be filtered out when a glitch filter value of >1 is specified, but it would be filtered out for a glitch filter value of >3 or >8.
Note: When the fast wake mode is enabled (
SYSOSC is requested asynchronously upon input pin activity), the ULPCLK will switch from off (as would be the case in STANDBY1) or 32kHz (as would be the case in STANDBY0) to 24Mhz/32MHz, resulting in the input synchronization logic and glitch filter running at 24Mhz/32MHz after some latency. See the device specific data sheet for the asynchronous fast clock request wake time, and budget this time into any minimum pulse width calculations when using fast wake.