SPRUJF2A March 2026 – March 2026 AM13E23019
This ADC has built-in support for oversampling in the first post-processing block(PPB1). The oversampling support module exists at the output of the sample correction module, as shown in Figure 15-8. The oversampling module works by accumulating results in partial registers until either the sample count limit defined in the ADCPPBxLIMIT register is reached , an external hardware sync event occurs, or the software forces a sync event by writing to the SWSYNC bit in the ADCPPBxCONFIG2 register.