SPRUJF2A March 2026 – March 2026 AM13E23019
The cipher block chaining (CBC) cipher mode builds upon the ECB cipher mode to make the ciphertext output for each block dependent not only on the plaintext and the cipher key k, but also upon the ciphertext of the previous block. The CBC cipher is shown in Figure 29-3. Like ECB mode, the plaintext data is divided into 128-bit blocks. Unlike ECB mode, in CBC mode each new plaintext block is bit-wise XORed with the previous ciphertext block to create the input to the AES block cipher.
In CBC mode, an unpredictable initialization vector (IV) must be provided. The initialization vector is XORed with the first plaintext block, as there is no "previous" ciphertext block to XOR the first plaintext block with.
The AESADV accelerator supports automated CBC mode operation of more than 128 bits of data either through interrupts or through the use of DMA. Software interrupt-based multi-block handling uses the AES interrupt condition reported in the CPU_INT.IIDX.STAT field. If this field reads 0x2 (INPUTRDY), then the next block of input can be written (as 4 32-bit writes). If this field reads 0x1 (OUTPUTRDY), then the output block can be read (as 4 32-bit reads).
In DMA mode, CBC utilizes two DMA channels. Channel bound to DMA_TRIG0 is the input channel. Channel bound to DMA_TRIG1 is the output channel. The channels need to be configured to perform one 32-bit read/write per trigger.