SPRUJF2A March 2026 – March 2026 AM13E23019
The LATCHCLR signal holds the digital filter, synchronization block, and the latch output in reset (0) after the required delays. The LATCHCLR signal is activated in software using xLATCHCLR (x = H or L). The LATCHCLR signal can also be activated by MCPWMSYNCPER when xSYNCCLREN (x = H or L) is set. If a longer LATCHCLR signal is required, the EPWMBLANK signal can be used to extend the LATCHCLR signal by setting BLANKEN.
MCPWMxSYNCPER comes from the Time-Base submodule of the MCPWM, respectively. For a detailed description of how these two signals are generated, refer to the Time Base Counter Synchronization subsection in the Multi-Channel Pulse Width Modulator (MCPWM) chapter.
The MCPWMxSYNCPER signal that loads DACxVALA when COMPDACCTL[SWLOADSEL] = 1 is a level trigger load. If TBCTR and TBPRD of the MCPWM are both 0, MCPWMSYNCPER is held at level high and DACxVALA is loaded immediately from DACxVALS irrespective of the value of COMPDACCTL[SWLOADSEL]. Due to this, configure the MCPWM first before setting COMPDACCTL[SWLOADSEL] to 1.