SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The interrupts to be used by the IEEE 802.15.4 commands are listed in Table 26-80. Each interrupt may be enabled individually in the system CPU. Details for when the interrupts are generated are given in Section 26.5.4.
| Interrupt Number | Interrupt Name | Description |
|---|---|---|
| 0 | COMMAND_DONE | A background level radio operation command has finished. |
| 1 | LAST_COMMAND_DONE | The last background level radio operation command in a chain of commands has finished. |
| 2 | FG_COMMAND_DONE | A foreground radio operation command has finished. |
| 3 | LAST_FG_COMMAND_DONE | The last foreground radio operation command in a chain of commands has finished. |
| 4 | TX_DONE | Transmitted frame |
| 5 | TX_ACK | Transmitted automatic ACK frame |
| 16 | RX_OK | Frame received with CRC OK |
| 17 | RX_NOK | Frame received with CRC error |
| 18 | RX_IGNORED | Frame received with ignore flag set |
| 22 | RX_BUF_FULL | Frame received that did not fit in the TX queue |
| 23 | RX_ENTRY_DONE | TX queue data entry changing state to Finished |
| 29 | MODULES_UNLOCKED | As part of the boot process, the Arm Cortex-M0 processor has opened access to RF core modules and memories. |
| 30 | BOOT_DONE | The RF core CPU boot is finished. |
| 31 | INTERNAL_ERROR | The radio CPU has observed an unexpected error. |